X-Cube MCSDK 6.2.0 and 6.2.1
Dear Sir/Madam ,
I am currently using MCSDK 6.1.0 for generating BLDC motor control project for various type of BLDC motors in both FOC mode and HALL sensor mode operations. Today I have tried to regenerate an existing BLDC motor control project in HALL Sensor mode using MCSDK 6.2.1 for the evaluation board EVSPIN32F0251S1. I have build the project in ST Cube IDE 1.14.1 and downloaded the code to the evaluation board. Then I have tried to start the motor in speed mode using ST Motor Pilot program. I have no problem in communication with the board. I made several trials , the motor starts moving but I got over current, over voltage , and mostly speedfeedback faults. The same thing happens with MCSDK 6.2.0 also . The system under test draws high current from the power source during the start-up phase when I start the motor. It seems to me , high side and low side mosfets activated at the same time.
I have no problem with same project settings in MCSDK 6.1.0 .