X-NUCLEO-IHM07M1 MC WORKBENCH Fault Problem
Greetings.
I started to study motor control with X-NUCLEO-IHM07M1 as following
- MCU : STM32F302R8
- PowerBD : X-NUCLEO-IHM07M1
- Motor : Bull Running BR2804-1700Kv
I just try to make STM32Cube IDE project using MC Workbench 6.4.1 (as described following screenshot image)

but, Using ST Motor Pilot, When start command is on, just motor starts rotate 1 cycle, and stopped. Then, Status Occurs "FAULT_OVER" as following screen image

And, main function is no codes for opreating because of just test with ST Motor pilot

Can I ask help for what is problem?
As Using MC Workbench Version 5.4.8, motor works.
Is any difference between MC Workbench 5.4.8 and 6.4.1?