Skip to main content
Best answer by Imen.D

Hello @Suthan ,

You can connect X-NUCLEO-IHM08M1 to the NUCLEO-H533RE (Nucleo-64 board) and mount the Arduino UNO R3 connectors.

1 reply

Imen.DBest answer
Technical Moderator
October 29, 2025

Hello @Suthan ,

You can connect X-NUCLEO-IHM08M1 to the NUCLEO-H533RE (Nucleo-64 board) and mount the Arduino UNO R3 connectors.

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
SuthanAuthor
Associate II
October 29, 2025

I was trying to use Motor Control Workbench, but I do not see H533RE in the control section? 

Also is that possible to add BLDC motor?

Suthan_0-1761750037429.png

 

GMA
Technical Moderator
October 30, 2025

Hello @Suthan,

As mentioned in the Release Note document available through Workbench tool > About > Documentations > Release Notes, the STM32H5 MCUs supported by MCSDK Workbench are:

  • STM32H5xx Family: STM32H503x, STM32H562x, STM32H563x, STM32H573x

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA