IBUUI.inf driver fails to install when using IBUUI Board Updater
Hi,
I am trying to use a STEVAL_PCC009V2 board connected to a EVAL6474H board to drive a stepper motor.
When I run the SPIN eval software I get a notice that the firmware is not the latest and I need to update it. I just ordered the board, but it shows as FW0.0. I have a ST-Link/V2 to program with, so I downloaded the IBUUI Board Updater, but it fails when I start the program with an error installing IBUUI.inf driver and exits.
I need to get this up and running ASAP so I can use it to move a stepper motor to evaluate the L6474.