Skip to main content
Visitor II
January 20, 2024
Question

Decoder for LoRa messages for Datacake

  • January 20, 2024
  • 1 reply
  • 1062 views

Hello,

I followed the indtructions from here, https://www.youtube.com/watch?v=vuc6914B0KM and I setup the NUCLEO-WL55JC STM32WL Nucleo-64 board and sensor board X-NUCLEO-IKS01A3 with LoRaWAN Gateway P-NUCLEO-LRWAN2 through The Things Network (TTN).

In this moment I am able to see the raw data in TTN Live data watch.

In the youtube 5 video example, the autor use the Cayenne app to create dashboard in order to decode and siaplay the sensor data.

Now, the issue is this: Cayenne is no more available, could you provide a Decoder code in JSON format for uplink and downlink, for application example LoRaWAN_End_Node?

Thank you,

Mihai

1 reply

STTwo-32
Technical Moderator
September 25, 2024

Hello @MihaiMEC 

No need for a modification on the Code of the LoRaWAN_End_Node. You can keep using the DATACAKE for example or the Zafron platform that can receive the same data frame as on Cayenne. 

Best Regards.

STTwo-32