AES encryption not working
Dear Team,
I want use inbuild AES encryption engine to encrypt the data, therefore I used CubeMX to initialize the AES engine, when i'm going to encrypt the payload, it stuck in
static HAL_StatusTypeDef CRYP_WaitOnOFNEFlag(CRYP_HandleTypeDef *hcryp, uint32_t Timeout) and return HAL_Error.
Kindly let me know what wrong am I doing to initialize the AES engine.
MCU = STM32F417VET
/********************* Code ****************************/
static void MX_CRYP_Init(void)
{
hcryp.Instance = CRYP;
hcryp.Init.DataType = CRYP_DATATYPE_8B;
hcryp.Init.pKey = (uint32_t *)pKeyCRYP;
hcryp.Init.pInitVect = (uint32_t *)pInitVectCRYP;
hcryp.Init.Algorithm = CRYP_DES_CBC;
hcryp.Init.DataWidthUnit = CRYP_DATAWIDTHUNIT_BYTE;
if (HAL_CRYP_Init(&hcryp) != HAL_OK)
{
Error_Handler();
}
}
HAL_CRYP_Encrypt(&hcryp, input, sizeof(input), output, 1000);