AES-GCM Chunk-Size 1
Hello,
I'm using AES-GCM using the method cmox_cipher_append() function call, as taken from the example below, taken from Projects\NUCLEO-L476RG\Applications\Cipher\AES_GCM_AEAD_EncryptDecrypt\Src\main.c
The code works well if the CHUNK_SIZE size is a multiple of 16. However, I want to decipher streamed data that comes in unpredictable chunks. I know that there is no limitation from the AES-GCM algorithm side on the CHUNK_SIZE. Is there a workaround to implement something with a CHUNK_SIZE of 1?