Skip to main content
kajtek610
Associate II
May 11, 2018
Question

AES128 HW_TIMEOUT error code

  • May 11, 2018
  • 0 replies
  • 627 views
Posted on May 11, 2018 at 14:41

Hi!

I'm struggeling with hardware accelerated aes algorythim. Based on example project I've enabled CRC clock and initilzed the operation, by passing the key (AccHw_AES_CFB_Encrypt_Init(&, , )). After that I'm trying encrypt data, but the function AccHw_AES_CFB_Encrypt_Append(&, , , ,&) return an error status HW_TIMEOUT. I set up a GCC compiler in AccHw_config.h witout any optimalization.  Floating point hardware with hard ABI has been set up as well. Oh and I'm using libSTM32AccHwCryptoV3.0.0__GCC_FPU.a libaries, STM32F429I-DISC1 discovery kit and SW4STM32 as a IDE.

If anyone of you guys has some idea what should be checked or done for fix the issue,

I will be grateful for any help

.

#hw_timeout #acc_hw #aes
This topic has been closed for replies.