Application hangs when doing a remote update
The details of this project are like this.
I have a working product on the F417 that I wish to add Remote update capabilities to.
Product is already deployed with SBSFU and updates using Ymodem through the UART work fine.
What I am trying to add on now is the Remote firmware update, which is based on the STM32CubeExpansion_Cloud_AZURE_V1.2.1, to be able to download the F/W from a webserver for an update.
What is puzzling me now is this:
When I test out the downloading in my debug build (without SBSFU) the .sfb file can be downloaded and saved to flash. I can peek into the flash with the debugger and see that the file has been saved.
However, when I build a release version (which is together with the SBSFU) and trigger the update process, when attempting to write to the flash, the program gets stuck and hangs at the HAL_FLASH_Program call and will eventually result in a watchdog reset.
I am baffled as to why I can write in debug mode but not in release mode. Why is there a difference in how the board runs in debug and release?