Skip to main content
Associate
October 29, 2025
Question

Cannot Connect to STM32H533 After Debug Authentication (Access Port Error)

  • October 29, 2025
  • 3 replies
  • 207 views

I’m working with a NUCLEO-H533RE board (STM32H5 series, TrustZone enabled) and using ST-LINK for debugging.

Here is the issue:

  • Debug Authentication succeeds (certificate-based).
  • Immediately after, the tool disconnects and shows:
Error: Unable to get core ID
Error: Cannot connect to access port 1! If you are trying to connect to a device with TrustZone enabled please try to connect with HotPlug mode. If you are trying to connect to a device which supports Debug Authentication with certificate and password, please open your device using it.
  • Log shows:
SDMAuthenticate: Authentication successful
Debug Authentication Success
Disconnected from device.
ST-LINK FW: V3J16M8
Board: NUCLEO-H533RE
Voltage: 3.28V
  • ST-Link configuration:
    • Port: SWD
    • Mode: HotPlug
    • Access Port: 0
    • Reset Mode: Software Reset
    • SWD Frequency: 8000 kHz
    • Shared: Disabled

I've tried:

  • HotPlug Mode as recommended for TrustZone.
  • Debug Authentication with valid certificate and key.
  • ST-Link firmware is up to date.

Still, after authentication, I cannot connect to the core or AP.

Questions:

  1. Why does the session drop immediately after authentication?
  2. Is this related to TrustZone or Option Bytes (Debug permissions)?
  3. Should I use “Connect under reset” instead of HotPlug?
  4. Which Access Port (AP0 vs AP1) should I select for STM32H533?

Any guidance or known working configuration for STM32H5 with Debug Authentication would be appreciated!

 

3 replies

Technical Moderator
October 30, 2025

Hello @elby0 

Welcome to the Community.

Maybe this post could be helpful to you: stm32h533 production state closed firmware not running.

Implementing debug authentication on STM32H5 using CLI tools

 

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
Jocelyn RICARD
ST Employee
November 11, 2025

Hello @elby0 ,

There shouldn't be any issue. At least I've never seen such behaviour.

Did you manage to recover?

Best regards

Jocelyn

elby0Author
Associate
November 11, 2025

Hello @Jocelyn RICARD 

 

No not yet. I still have the same issue. I didn't look at this in the last few weeks as I had other priorities but I will get back to you when I have the chance to look into this.

 

Regards

elby