Cannot debug the AWS demo on B-L475E-IOT01A1
Dear all,
For an IoT project I would like to run the demo of the AWS package provided by ST but for some reason I could not manage to debug the demo project.
To do so I have downloaded the X-CUBE-AWS_v2.0.0 package and used the following ressources :
Before trying to run in debug mode the project I did the following steps :
- created a thing on AWS
- created a certificate/private key on AWS
- provisionned the certificate and private key to aws_clientcredential_keys.h (I don't want to use the ST-SAFE here)
- provided connection information into aws_clientcredential.h
Then prepared the SBSFU :
- Built the project B-L4S5I-IOT01_2_Images_SECoreBin.
- Built the project B-L4S5I-IOT01_2_Images_SBSFU
Then prepare the demo project :
- I merge the demo project with the AWSxSTM32 workshop sensor example to get the sensor streaming of the proto board to AWS.
- I build the demo project. I had to apply the following fix provided by @Jocelyn RICARD
- Using STM32CubeProgrammer, I flashed the .bin file successfully. Note that I did not prepared a .sfb file for testing OTA yet.
Finally I configured and launched the debug configuration with the following details :
- Into Load Image and Symbols > uncheck Download
- Into Runtime Options > Check Set Program Counter : 0x08000000
Unfortunately, when I finally run the demo app I run into these error logs in the console :
Open On-Chip Debugger 0.11.0-rc2+dev-00037-g4c4dbd9 (2021-02-09-13:36)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V2J37M27 (API v2) VID:PID 0483:374B
Info : Target voltage: 3.217860
Info : clock speed 5 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x2ba01477
Info : STM32L4S5VITx.cpu: hardware has 6 breakpoints, 4 watchpoints
Info : STM32L4S5VITx.cpu: external reset detected
Info : starting gdb server for STM32L4S5VITx.cpu on 3333
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
target halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x081073cc msp: 0x2009fffc
Info : device idcode = 0x10076415 (STM32L47/L48xx - Rev 4 : 0x1007)
Info : RDP level 0 (0xAA)
Info : flash size = 1024kbytes
Info : flash mode : dual-bank
Warn : negative reply, retrying
Warn : negative reply, retrying
Info : accepting 'gdb' connection on tcp/3333
target halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x081073cc msp: 0x2009fffc
Warn : keep_alive() was not invoked in the 1000 ms timelimit. GDB alive packet not sent! (3889 ms). Workaround: increase "set remotetimeout" in GDB
Warn : negative reply, retrying
Warn : negative reply, retrying
Error: can't add breakpoint: unknown reason
Error: can't add breakpoint: unknown reasonOf course, I have not enabled any breakpoint so I don't know what to do !
Does someone has any suggestion ?
Thank you in advance for your help ! :)
EDIT :
I tried to do a fresh start with the ST starting guide for X-CUBE-AWS_v2.2.0
The bootloader compiles well and the demos_osc project as well. However, the demos_osc resulting .elf files weight 4MB but the CPU only has 1MB of FLASH.
What can be the cause of this problem in the example project ?