debug OEMiRoT-Boot project on U083 possible?
I'm aiming to use the OEMiRoT sample project as a concept for secure updating of a large single-slot application in STM32U083 (need application size at least 160kB for migration from STM32L071). For that I need to give the bootloader a driver for external SPI flash where the encrypted updates can reside that the application downloads.
The How_to_start_with_OEMiRoT_on_STM32U0 manual doesn't address the concept of debugging OEMiRoT at all. The provisioning procedure works, using RDP level 0 (even with modified code, as I can see an error printout that I added in the bootloader init).
Starting a debugging session after this provisioning results in the debugger not being able to erase the sectors, on the other hand after erasing the chip beforehand (using ob_flash_programming.bat upto the erase part) it succeeds and I can debug, but immediately run into the protection mechanisms generating errors.
Is there any manual how to debug this project and which defines to disable/modify to debug the low level drivers before activating all protections again? To my surprise there isn't even a difference in preprocessor defines for the debug and release builds to automatically disable some of these protections in the debug build.