DIfference in results based on different AES mode
If I use AES mode CRYP_CR_ALGOMODE_AES_CBC, the decryptedText array does not match with the last 3 uint32_t values in the array. Same goes with ECB mode. However, when GCM or CCM modes are used, the decrypted data is same as the plain text. I could not find any hints in the errata sheet either.
Has anyone else faced a similar problem?
#define BUFF_LEN 15
uint32_t AES256Key[8] = {0xB374A26A, 0x71490437, 0xAA024E4F, 0xADD5B497,
0xFDFF1A8E, 0xA6FF12F6, 0xFB65AF27, 0x20B59CCF};
uint32_t InitVector[4] = {0x7E892875, 0xA52C59A3, 0xB588306B, 0x13C31FBD};
uint32_t Ciphertext[BUFF_LEN] = {0x42831ec2, 0x21777424, 0x4b7221b7, 0x84d0d49c,
0xe3aa212f, 0x2c02a4e0, 0x35c17e23, 0x29aca12e,
0x21d514b2, 0x5466931c, 0x7d8f6a5a, 0xac84aa05,
0x1ba30b39, 0x6a0aac97, 0x3d58e091};
uint32_t Plaintext[BUFF_LEN] = {0xd9313225, 0xf88406e5, 0xa55909c5, 0xaff5269a,
0x86a7a953, 0x1534f7da, 0x2e4c303d, 0x8a318a72,
0x1c3c0c95, 0x95680953, 0x2fcf0e24, 0x49a6b525,
0xb16aedf5, 0xaa0de657, 0xba637b39};
uint32_t Encryptedtext[BUFF_LEN] = {0};
uint32_t Decryptedtext[BUFF_LEN] = {0};
int main() {
CRYP_HandleTypeDef hcryp1;
memset((CRYP_HandleTypeDef *)&hcryp1, 0x00, sizeof(CRYP_HandleTypeDef));
hcryp1.Instance = CRYP;
hcryp1.Init.DataType = CRYP_DATATYPE_32B;
hcryp1.Init.KeySize = CRYP_KEYSIZE_256B;
hcryp1.Init.pKey = AES256Key;
hcryp1.Init.Algorithm = CRYP_CR_ALGOMODE_AES_CBC;
hcryp1.Init.pInitVect = InitVector;
HAL_CRYP_Init(&hcryp1);
HAL_CRYP_Encrypt(&hcryp1, Plaintext, BUFF_LEN, Encryptedtext, TIMEOUT_VALUE);
HAL_CRYP_Decrypt(&hcryp1, Encryptedtext, BUFF_LEN, Decryptedtext,
TIMEOUT_VALUE);
HAL_CRYP_DeInit(&hcryp1);
if (memcmp(Decryptedtext, Plaintext, 60) != 0) {
/* Not expected result, wrong on Encryptedtext buffer: Turn LED3 on */
// Error_Handler();
}
}