Question
Does HAL_FLASH_OB_Launch cause a system reset on STM32H563 MCU?
As for STM32H563 MCU, will it result in a system reset after executing the function HAL_FLASH_OB_Launch?
From my experiment, before executing HAL_FLASH_OB_Launch, I can read data from MCU via I2C while all returned data become 0xFF(i.e. invalid data) after executing this function.
It seems that the MCU is suspended or reset. When I tried to trace the code through Debugger Section in Keil, the code can run smoothly to subsequent routines.
Here is my code below.
void EnableWriteProtect(uint8_t image)
{
FLASH_OBProgramInitTypeDef OBInit = {0};
FLASH_OBProgramInitTypeDef sOBPrev = {0};
uint32_t WRPSector;
/* Unlock the User Flash area */
HAL_FLASH_Unlock();
HAL_FLASH_OB_Unlock();
/* Get the boot configuration status */
HAL_FLASHEx_OBGetConfig(&OBInit);
WRPSector = OBInit.WRPSector | BIT(0);
OBInit.Banks = FLASH_BANK_2;
OBInit.OptionType = OPTIONBYTE_WRP;
OBInit.WRPState = OB_WRPSTATE_ENABLE;
OBInit.WRPSector = WRPSector;
HAL_FLASHEx_OBProgram(&OBInit);
/* Launch Option bytes loading */
HAL_FLASH_OB_Launch();
/* Unlock the User Flash area */
HAL_FLASH_Lock();
HAL_FLASH_OB_Lock();
}
My expectation: I hope to implement write protection for specific MCU flash areas normally without resetting the MCU.