EEPROM and mass erase when moving from LEVEL1 to LEVEL0
Hi there,
I'm under mass production with yours STM32L051x8 device.
I use the internal EEPROM to keep some data. Note that is not en emulation eeprom on flash, is just 512bytes on internal EEPROM.
In addition, I protect my code with ReadOutProtection Level =1.
Seems that when I update the version of customer firmware, the EEPROM data is erased. Seems that jumping from Level1 to Level0 produce a mass erase, and in consequence, the EEPROM is erased as well.
I would like to know if I'm right.
Jumping from Level1 to Level0 produce a mass erase, that produce erase the internal EEPROM as well?
Thanks a lot.