Enable readout protection using system memory bootloader
I have been using the STM32 serial bootloader, instead of coding my own bootloader, for a while now. But lately I wanted to protect my code, so I tried to enable readout protection (RDP) level 1. This is meant to prevent the user to read the flash.
However, after a few attempts, it seems that it is not possible to use this sytem memory bootloader to enable RDP, then start running the code that I put in the flash.
From what I understand, running the flash is considered "debugging" access, and is prevented when RDP is active. Is there a way to get around this ? I would like to protect my code from "basic" read access (like JTAG) without coding my own bootloader
Thanks