Errors building TFM example for U545
Hi, I'm trying to build TFM example applications from the B-U585I-IOT02A directory to work on Nucleo-U545RE board. THe documentation says it's possible. I have updated the project settings, but I'm getting errors from the STSAFE library:
C:/Work/OldCourse/SecureBootTesting_ST/Projects/B-U585I-IOT02A/Applications/TFM/TFM_Appli/Secure/Src/stsafea_service_interface.c:92:51: warning: implicit declaration of function '__HAL_RCC_GPIOF_CLK_ENABLE' [-Wimplicit-function-declaration]
92 | #define STSAFEA_VREG_GPIO_PORT_CLK_ENABLE __HAL_RCC_GPIOF_CLK_ENABLE
| ^~~~~~~~~~~~~~~~~~~~~~~~~~
C:/Work/OldCourse/SecureBootTesting_ST/Projects/B-U585I-IOT02A/Applications/TFM/TFM_Appli/Secure/Src/stsafea_service_interface.c:301:3: note: in expansion of macro 'STSAFEA_VREG_GPIO_PORT_CLK_ENABLE'
301 | STSAFEA_VREG_GPIO_PORT_CLK_ENABLE();
| ^~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
C:/Work/OldCourse/SecureBootTesting_ST/Projects/B-U585I-IOT02A/Applications/TFM/TFM_Appli/Secure/Src/stsafea_service_interface.c:91:51: error: 'GPIOF' undeclared (first use in this function); did you mean 'GPIOG'?
91 | #define STSAFEA_VREG_GPIO_PORT GPIOF
| ^~~~~
The problem seems to be coming from the fact that this MCU does not have GPIOF port. Instead of editing the file I would prefer to disable the STSAFE altogether, because I have no intention of using it.
I tried to remove the STSAFE_A110 definition, but then I got more compilation errors.
Also tried to set TFM_PSA_API to zero, but it didn't change anything.
Is there an official way to disable STSAFE?