Skip to main content
Associate II
March 14, 2025
Question

External Flash Loader with Secure Flash

  • March 14, 2025
  • 2 replies
  • 722 views

In my project, I intend to use an external serial flash to hold UI assets as recommended by TouchGFX.

I have followed this: https://community.st.com/t5/stm32-mcus/how-to-implement-and-use-your-own-external-flash-loader-an/ta-p/597752 but I only get flash erase errors from the STM32CubeProgrammer.

The main issue that I see is that this project also needs to have the secure flash feature active, which is where I believe that the problem lies.

Does anyone know if external flash loaders works with Secure Flash enabled? If so is there a white paper or document describing how to make both work?

Thank you.

2 replies

Technical Moderator
March 17, 2025

Hello @RW3562 

Very interesting use case that I will share internally. I need more details:

"Does anyone know if external flash loaders works with Secure Flash enabled?" can you share the reference of the external secure Flash ?

Best Regrds

RW3562Author
Associate II
March 21, 2025

Hi CMYL,

The external flash is a common N25Q128A flash. It's the internal flash on the STM32U5 that's secured - which I'm assuming could be blocking access to the external flash.

Thanks

KDJEM.1
Technical Moderator
March 17, 2025

Hello @RW3562 and welcome to the community;

 

"The main issue that I see is that this project also needs to have the secure flash feature active, which is where I believe that the problem lies." 

I don't think the erase issue is related to flash secure.

Which memory are you using?

Could you please check the memories characteristics in Dev_Inf.c file? 

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
RW3562Author
Associate II
March 21, 2025

Hello Kaouthar

I'm using a N25Q128A external flash.

The contents of Dev_Inf.c is:

struct StorageInfo const StorageInfo = {
"my-board-loader", // Device Name + EVAL Borad name
NOR_FLASH, // Device Type
0x90000000, // Device Start Address
0x01000000, // Device Size
0x1000, // Programming Page Size
0xFF, // Initial Content of Erased Memory
// Specify Size and Address of Sectors (view example below)
0x00000100, 0x00010000, // Sector Num : 1024 ,Sector Size: 64 KBytes
0x00000000, 0x00000000,
};

The truth is that I don't know what is causing the failure, so I assumed that since the internal flash on the STM32U5 is protected with secure flash, the access to peripheral hardware could also been blocked by the secure flash protection.