Have the scripts included in the MOOC's package changed?
Dear Sirs,
I have downloaded and installed the
package. I am able to build the example projects with CubeIDE flawlessly but
the batch scripts (.bat) are not working.
running the scripts
(e.g.02_01_Postbuild_SimpleAppV1.bat) I get the error "The specified path
cannot be found." (actually the message is in the system language, that in
my case is Italian, so I am not 100 % sure of the translation in English
language).
Trying to look into the batch script, it
is truing to access this folder:
set "prepareimage=%basedir%\win\prepareimage\prepareimage.exe"
But after installing the MOOC package
(with the installer "STM32SecuWS-material.exe"), I can not find any
"win" directory in any location.
Am I missing g something?
Thank
you.
Kind
regards,
Claudio