Skip to main content
FOCal.1
Visitor II
May 26, 2022
Question

Hi, is there a full reference document for the prepareimage (Win exe or Python) tool, which is used in the SBSFU package? I see some examples but I'd like to be able to look up detailed information on the various parameters.

  • May 26, 2022
  • 1 reply
  • 1622 views

I do have the document UM2262 which describes the SBSFU expansion package, but it only gives a fairly brief explanation of the prepareimage tool.

1 reply

Jocelyn RICARD
ST Employee
June 29, 2022

Hello @FOCal.1​ ,

there is no specific document related to this tool.

You can launch python prepareimage.py -h to get all commands

You can also get help for each command using prepareimage.py <cmd> -h

For instance:

python prepareimage.py keygen -h
usage: prepareimage.py keygen [-h] -k filename -t type
 
optional arguments:
 -h, --help show this help message and exit
 -k filename, --key filename
 -t type, --type type

But to get the possible types for this specific command, you will need to check inside prepareimage.py:

... 
 keygenp.add_argument('-t', '--type', metavar='type',
 choices=['aes-gcm', 'ecdsa-p256','aes-cbc','aes-ctr'],
 required=True)
...

Best regards

Jocelyn

Visitor II
July 2, 2024

Hello @Jocelyn RICARD ,

Can you please elaborate on the meaning of "outfile" and "offset file". 

 

 diff.add_argument('-1', '--file1', type=str, metavar='filename', required=True, help="first binary file to compare")
 diff.add_argument('-2', '--file2', type=str, metavar='filename', required=True, help="second binary file to compare")
 diff.add_argument('-p', '--poffset', type=str, metavar='filename', required=True, help="file that will contain offset at which the difference binary files should be applied")
 diff.add_argument('-b', '--begin', type=auto_int, metavar='filename', default='0x0', required=False, help="offset from which beginning comparison - in bytes (default: 0)")
 diff.add_argument('-e', '--end', type=auto_int, metavar='filename', default='0x0', required=False, help="offset at which ending comparison - in bytes. use 0 to specify end of given binary files (default: 0)")
 diff.add_argument('-a', '--align', type=int, metavar='align', default=2, required=False, help="difference binary file alignment in bytes (default: 2)")
 diff.add_argument("outfile")