Skip to main content
Markus Arzl
Visitor II
May 11, 2018
Question

high numeric performance, secure boot and USB FS or ethernet combinbed?

  • May 11, 2018
  • 0 replies
  • 566 views
Posted on May 11, 2018 at 09:39

Hello,

we are are looking for a microprocessor or microcontroller with the following features:

o USB FS or ethernet connectivity, ( USB FS preferred)

o high processing power >= 700MHz, multi core if possible

o secure and protected flash for our program binaries

I understand, that high performance calculations and on chip flash don't match that well, but maybe somebody has heard of a solution for this dilemma?

One main point is that we need to have our firmware well protected. External flash solutions seem to fail on this requirement...

Can somebody please give me a clue?

Thanks in advance!

Markus

#secure-boot #performance
    This topic has been closed for replies.