How to Program stm32f103rc using j-Link when RDP enabled?
Hello.
I'm trying to program the main flash memory of STM32F103RCT6 using J-Link while RDP is enabled.
I followed main flash memory programming procedure in PM0075 manual.
the procedure is in below picture.
When only RDP is enabled, I unlocked Flash_CR_LOCK bit and then Write FLASH_CR_PG to 1.
After this procedure, I tried to write half-word data to 0x080069f0.
However, J-Link reports the error like this.
****** Error: Timeout while calculating CRC, RAMCode did not respond in time. (PC = 0x00000000, CPSR = 0x00000000, LR = 0x01000000)!Failed to erase sectors 14 @ address 0x08006800 ((erase error))
Failed to erase sectors.
Is it impossible to program main flash memory when RDP is enabled?
If not, how can I do it?
Here is my J-Link Commander log.
Device "STM32F103RC (ALLOW OPT. BYTES)" selected.
Connecting to target via JTAG
InitTarget() start
Active read protection detected.
Skipping unsecure.
InitTarget() end
TotalIRLen = 9, IRPrint = 0x0011
JTAG chain detection found 2 devices:
#0 Id: 0x3BA00477, IRLen: 04, CoreSight JTAG-DP
#1 Id: 0x06414041, IRLen: 05, STM32 Boundary Scan
DPv0 detected
Scanning AP map to find all available APs
AP[1]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x14770011)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FF000
CPUID register: 0x411FC231. Implementer code: 0x41 (ARM)
Found Cortex-M3 r1p1, Little endian.
FPUnit: 6 code (BP) slots and 2 literal slots
CoreSight components:
ROMTbl[0] @ E00FF000
ROMTbl[0][0]: E000E000, CID: B105E00D, PID: 001BB000 SCS
ROMTbl[0][1]: E0001000, CID: B105E00D, PID: 001BB002 DWT
ROMTbl[0][2]: E0002000, CID: B105E00D, PID: 000BB003 FPB
ROMTbl[0][3]: E0000000, CID: B105E00D, PID: 001BB001 ITM
ROMTbl[0][4]: E0040000, CID: B105900D, PID: 001BB923 TPIU-Lite
ROMTbl[0][5]: E0041000, CID: B105900D, PID: 101BB924 ETM-M3
Cortex-M3 identified.
J-Link>w4 40022004 45670123
Writing 45670123 -> 40022004
J-Link>w4 40022004 cdef89ab
Writing CDEF89AB -> 40022004
J-Link>mem32 40022010 1
40022010 = 00000000
J-Link>h
PC = 08003FFE, CycleCnt = 3A8FCF29
R0 = E000ED0C, R1 = 05FA0004, R2 = 05FA0004, R3 = 40003000
R4 = 20000924, R5 = 1FFFF810, R6 = 1FFFF810, R7 = 2000BFDC
R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000
R12= 00000000
SP(R13)= 2000BFDC, MSP= 2000BFDC, PSP= 00000000, R14(LR) = FFFFFFF9
XPSR = 01000003: APSR = nzcvq, EPSR = 01000000, IPSR = 003 (HardFault)
CFBP = 00000000, CONTROL = 00, FAULTMASK = 00, BASEPRI = 00, PRIMASK = 00
FPU regs: FPU not enabled / not implemented on connected CPU.
J-Link>w4 40022010 0000001
Writing 00000001 -> 40022010
J-Link>w2 080069f0 1111
Writing 1111 -> 080069F0
J-Link>mem32 4002200c 1
****** Error: Timeout while calculating CRC, RAMCode did not respond in time. (PC = 0x00000000, CPSR = 0x00000000, LR = 0x01000000)!Failed to erase sectors 14 @ address 0x08006800 ((erase error))
Failed to erase sectors.