Skip to main content
asala.19
Associate III
April 17, 2020
Question

How to remove sbsfu code

  • April 17, 2020
  • 3 replies
  • 1465 views

Hi support team,

i am testing the sbsfu code in P-NUCLEO-WB55 but i missed out to disable security ips SECBOOT_DISABLE_SECURITY_IPS and flash into the board it set RDP level to 1 also set SFU_WRP_PROTECT_ENABLE, SFU_TAMPER_PROTECT_ENABLE,SFU_DAP_PROTECT_ENABLE,SFU_MPU_PROTECT_ENABLE... .

now i want to remove this code and flash other application but i can not debug or run as application via IDE(AC6 or cubeide) it through error: write protection detected check RDP and WRP protection options.

Please help me out to resolve above issue.

I have change RDP from 1(BB) to 0(AA) but issue is not resolve.

Thanks,

Arjun

This topic has been closed for replies.

3 replies

alister
Senior III
April 17, 2020

Per RM0433 and UM2262 and others...

An RDP L0 regression from L1 performs a mass-erase.

So you have to connect a ST-LINK or similar, change the RDP to level 0 (which does the mass-erase) and disable the WRPs.

This leaves user flash empty.

Then you have to re-load the combined SBSFU and app, or just the SBSFU and use it to re-load the app.

asala.19
asala.19Author
Associate III
April 17, 2020

Hi @alister​ 

Thanks for your support resolve the issue by changing WRP1A_START and WRP1A_END (WRPxy_START > WRPxy_END = No WRP or unprotected, as mentioned in RM0434 ).

Thanks,

Arjun

asala.19
asala.19Author
Associate III
April 17, 2020

Hi @alister​ 

Thanks for quick response i am using stcubeprogrammer for change RDP level, it change successfully from 1 to 0 but i can't find how to disable WRPs

please find attached image0693W000000W07zQAC.png

Thanks,

Arjun

alister
Senior III
April 17, 2020

STM32CubeProgrammer isn't intuitive. You'll have to check RM0434 and try to correlate its description of WRP with this GUI.

Alternatively, if you have an older tool called "STM32 ST-LINK Utility", that was pretty easy to understand.

jarus0
Associate II
December 22, 2022

Hello Everyone, I'm in exactly the same situation.

I've changed RDP and WRPxy_START, WRPxy_END

Please find the values in the below log.

./STM32_Programmer_CLI -c port=swd -ob displ 
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.12.0 
 -------------------------------------------------------------------
 
ST-LINK SN : 0671FF313736504157192620
ST-LINK FW : V2J40M27
Board : NUCLEO-G070RB
Voltage : 3.22V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x460
Revision ID : Rev B
Device name : STM32G07x/STM32G08x
Flash size : 128 KBytes
Device type : MCU
Device CPU : Cortex-M0+
BL Version : 0xB2
Debug in Low Power mode enabled
 
 
UPLOADING OPTION BYTES DATA ...
 
 Bank : 0x00
 Address : 0x40022020
 Size : 112 Bytes
 
[==================================================] 100% 
 
 
OPTION BYTES BANK: 0
 
 Read Out Protection:
 
 RDP : 0xAA (Level 0, no protection) 
 
 BOR Level:
 
 BOR_EN : 0x0 (Configurable brown out reset disabled, power-on reset defined by POR/PDR levels) 
 BORR_LEV : 0x0 (BOR rising level 1 with threshold around 2.1 V) 
 BORF_LEV : 0x0 (BOR falling level 1 with threshold around 2.0 V) 
 
 User Configuration:
 
 nRST_STOP : 0x1 (No reset generated when entering Stop mode) 
 nRST_STDBY : 0x1 (No reset generated when entering Standby mode) 
 nRST_SHDW : 0x1 (No reset generated when entering the Shutdown mode) 
 IWDG_SW : 0x1 (Software independant watchdog) 
 IWDG_STOP : 0x1 (IWDG counter active in stop mode) 
 IWDG_STDBY : 0x1 (IWDG counter active in standby mode) 
 WWDG_SW : 0x1 (Software window watchdog) 
 RAM_PARITY_CHECK: 0x1 (SRAM parity check disable) 
 nBOOT_SEL : 0x1 (BOOT0 signal is defined by nBOOT0 option bit) 
 nBOOT1 : 0x1 (Boot from Flash if BOOT0 = 0, otherwise system memory) 
 nBOOT0 : 0x1 (nBOOT0=1) 
 NRST_MODE : 0x3 (Bidirectional reset: NRST pin configured in reset input/output mode (legacy mode)) 
 IRHEN : 0x1 (Internal resets drives NRST pin low until it is seen as low level) 
 
 PCROP Protection:
 
 PCROP1A_STRT : 0xFF (0x801FE00) 
 PCROP1A_END : 0x0 (0x8000200) 
 PCROP_RDP : 0x0 (PCROP zone is kept when RDP is decreased) 
 PCROP1B_STRT : 0xFF (0x801FE00) 
 PCROP1B_END : 0x0 (0x8000200) 
 
 Write Protection:
 
 WRP1A_STRT : 0x0 (0x8000000) 
 WRP1A_END : 0x0 (0x8000000) 
 WRP1B_STRT : 0x3F (0x801F800) 
 WRP1B_END : 0x0 (0x8000000) 
 
 FLASH security:
 
 BOOT_LOCK : 0x0 (Boot based on the pad/option bit configuration) 
 SEC_SIZE : 0x20 (0x8010000)

Let me know how to resolve this.