Skip to main content
SteveC
Associate
June 26, 2020
Question

I'm running Win10 in Fusion on a Mac. It detects the 552 but not the 476

  • June 26, 2020
  • 2 replies
  • 644 views

..

    This topic has been closed for replies.

    2 replies

    Jocelyn RICARD
    ST Employee
    June 26, 2020

    Hello Steve,

    this is a setup we cannot reproduce.

    Could you open the device manager ?

    Normally, when plugging a board, you should see the update.

    Also, when plugging the STM32L476 you should see the LED1 and LED3 active.

    Best regards

    Jocelyn

    SteveC
    SteveCAuthor
    Associate
    June 26, 2020

    SOLVED! When it first failed I change the USB lead. It didn't work with the second lead either. I should have tried a third lead! Now with a third lead everything is fine. Worth nothing that not all USB leads are the same! Thanks STM for your support :)