Implement Key replacement package for Image signing Key ECCKEY1
The SBSFU framework allows users to employ multiple image signing keys, ECCKEY1, ECCKEY2, and ECCKEY3.
Is there a method to blacklist ECCKEY1 and replace it with ECCKEY4, which may be transmitted via a key replacement update package if the private key for ECCKEY1 is leaked/compromised?
Keys are compiled into code and stored in the SE Key region ROM, which is secured by MPU-RX + WRP + PCROP.
Please advise what options I have to replace the key which is compromised?
Assuming bootloader enhanced to differentiate between .sfb and key replacement package.