Interrupt on UserApp not working with SBSFU
Hi everyone,
currently, I'm struggling to make interrupt working with SBSFU (STM32WB55).
If I run the program without SBSFU, interrupt event working properly.
but when I compiled it along with SBSFU, the interrupt not working.
I see on another post that is possibility its caused by interrupt vector.
I used this configuration on system_wbxx.c
#if defined(__ICCARM__)
extern uint32_t __vector_table;
#define INTVECT_START ((uint32_t)& __vector_table)
#elif defined(__CC_ARM) || defined(__ARMCC_VERSION)
extern void * __Vectors;
#define INTVECT_START ((uint32_t) & __Vectors)
#elif defined(__GNUC__)
extern void * g_pfnVectors;
#define INTVECT_START ((uint32_t)& g_pfnVectors)
#endif
actually, the program is running but interrupt still not working.
I also tried with this code:
#if defined(__ICCARM__)||defined(__GNUC__)
extern uint32_t __ICFEDIT_intvec_start__;
#define INTVECT_START ((uint32_t)& __ICFEDIT_intvec_start__)
#elif defined(__CC_ARM)
extern uint32_t Image$$vector_start$$Base;
#define INTVECT_START ((uint32_t)& Image$$vector_start$$Base)
#endif
the intterupt still not working.
Any advise? Thanks in advance