Skip to main content
Tim.N
Associate III
November 9, 2020
Solved

Is the CRC peripheral used by the FUS services on the STM32WB?

  • November 9, 2020
  • 3 replies
  • 1127 views

Hi -

I had been working on getting FUS support for upgrading images integrated into our firmware, and I discovered that my initialization of the CRC peripheral was causing the FUS subsystem to reject all upgrade attempts. I couldn't find any documentation inside AN5185 that indicated that the CRC peripheral was used for the FUS services, but could I get confirmation that it is indeed being used by FUS?

I can get FUS to succeed by resetting the CRC peripheral in my code before invoking (thus deinitializing the CRC peripheral) a FUS upgrade attempt.

If this is indeed the case that it requires the CRC peripheral, please update AN5185's table 3 "FUS resources usage".

Thanks,

Tim

This topic has been closed for replies.
Best answer by Christophe Arnal

​Hello,

CRC is used by the FUS during firmware update. the AN5185 is already planned to be updated but I dot have the released date.

Regards.

3 replies

Christophe ArnalBest answer
ST Employee
November 10, 2020

​Hello,

CRC is used by the FUS during firmware update. the AN5185 is already planned to be updated but I dot have the released date.

Regards.

Remi QUINTIN
Technical Moderator
November 10, 2020

​Yes I confirm that CRC is used by FUS indirectly. It seems to be used by CyrptoLib that is used by FUS. But this lib does not perform the initialization. Thus the FUS does it, which in a way is a bit peculiar.

Tim.N
Tim.NAuthor
Associate III
November 10, 2020

Thanks for the confirmation.