Skip to main content
yury
Associate III
June 23, 2017
Question

Jump to bootloader and Read out protection conflict

  • June 23, 2017
  • 2 replies
  • 1643 views
Posted on June 23, 2017 at 04:01

Hi everyone!

I'm using STM32F105 MCU , and I'd like to explore built-in DFU feature

When I set BOOT0/BOOT1 pins per datasheet and reboot the MCU, the feature always works ok no matter how read out protection is set in option bits

However, jump from application works only if read out protection is off

The jump code disables all IRQ sources used in my application, clears pending interrupts, sets stack top and jumps to system memory per AN2606

&sharpdefine _DFU_START (0x1FFFB000)

static void (*_p_ldr)(void);

NVIC_DisableIRQ(TIM2_IRQn);

NVIC_DisableIRQ(TIM3_IRQn);

NVIC_DisableIRQ(TIM4_IRQn);

NVIC_DisableIRQ(DMA1_Channel1_IRQn);

NVIC_ClearPendingIRQ(TIM2_IRQn);

NVIC_ClearPendingIRQ(TIM3_IRQn);

NVIC_ClearPendingIRQ(TIM4_IRQn);

NVIC_ClearPendingIRQ(DMA1_Channel1_IRQn);

HAL_RCC_DeInit();

HAL_DeInit();

_p_ldr = ( void(*)(void)) (*((uint32_t *)(_DFU_START+4)));

__set_MSP(*(__IO uint32_t*) _DFU_START);

_p_ldr();

What may cause the problem?

#dfu #bootloader #stm32 #read-out-protection
This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
June 23, 2017
Posted on June 23, 2017 at 04:11

I've generally advocated the use of NVIC_SystemReset() and a ma gic number in RAM so ResetHandler can quickly vector to the ROM in near reset conditions.

Check things like SysTick

Try setting SCB->VTOR to _DFU_START

Double check ROM address, not aware of ROP on FLASH precluding the reading or execution of ROM code. Should be able to read things like options bytes and unique serial, etc. The ROM is aware of ROP, and limits subset of feature available, I suppose that could be an issue.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
yury
yuryAuthor
Associate III
June 23, 2017
Posted on June 23, 2017 at 12:30

Thank you for your quick reply

Correct me if I'm wrong but the RAM location would contain random value upon normal startup, so there's very small yet finite probability of unintended branching to DFU, isn't ?

ROM address is just start of system memory like described in device datasheet and AN2606

What exactly should I do about SysTick and how can it be related to ROP? (keeping in mind that DFU works ok when activated by boot pins. Even if ROP is on).

Uwe Bonnes
Chief
June 23, 2017
Posted on June 23, 2017 at 12:41

It is a pity that only F04 and F07 have a 'Jump to Bootloader from application code' entry point!

yury
yuryAuthor
Associate III
June 23, 2017
Posted on June 23, 2017 at 12:50

Despite of that, jumping to start of system memory worked ok for me with STM32F042 devices, without the problem described in the starting post

Uwe Bonnes
Chief
June 23, 2017
Posted on June 23, 2017 at 13:40

Either you care to reset many settings, or a bare jump to bootloader will not work reliable in some situations. So caring for the right setup is best done in the bootloader!