Visitor II
November 23, 2021
Question
Linker error occurred in IAR 7.60 when compiling the XCUBE expansion package for NUCLEO-F411RE
- November 23, 2021
- 1 reply
- 1166 views
I am using IAR Embedded Workbench 7.60 and configuring the XCube-SBSFU extension package for Nucleo-F411RE.
I have done the Compilation in below order and the it is successful for Securebin & SBSFU project.
- Securebin
- SBSFU
- UserApp
When compiling the User App project, getting the below linker error for the following line in the .icf file .
define root section aes_block_padding with alignment = 16
{
udata8 "Force Alignment";
pad_to 16;
};
Error[Lc003]: expected "block", "memory", "movable", "overlay", "region", "sharing", or "symbol"
I don't understand the issue here. For reference, attached the file