PCROP Not disabled after RDP Regression, Option change not possible in RDP0
Hello everyone,
I'm experimenting PCROP activation on stm32h743 following this ST-tutorial: https://youtu.be/7Wr90XFA8_Q?si=tDpqUtMdin9Oyn-P
The activation works fine but i cannot disable PCROP using CubeProgrammer.
I did a RDP1 to RDP0 regression with DMWP1 checked but the PCROP is still active

After RDP regression i can se that the unprotected flash are is erase:

But not the protected one:

I can also not change the option bytes anymore, even RDP0 to RDP1 does not work

How can i recover from this situation ?