Porting of X-Cube-SBSFU to Nucleo H745
Hello, I am looking to port one the examples from X-CUBE-SBSFU to get it running on my Nucleo H745ZI-Q. For some background I am very new to the world of STM32 and STM32Cube and I am trying to learn to get this feature running on this nucleo board I am using.
I have looked through the document AN5056 and I dont entirely understand what I need to change to get the example running on my nucleo. I started off with trying to follow the steps in AN5056 and UM2262 using the project for NUCLEO-H753ZI in the SBSFU package. I chose this sample project as it seems to be the closest package to my nucleo H745 board.
I first added the projects for SECoreBin, SBSFU and UserApp to STM32CubeIDE. I updated the Tamper GPIO pin configuration in sfu_low_level_security.h to TAMPER2 since my board only has 2 tamper pins while the example was using 3. Then built all 3 of the projects in STM32CubeIDE. Following that I successfully downloaded the binary for SBSFU to my nucleo using STM32CubeProgrammer. After power cycling the board as described in the document, I connected to the serial monitor on TeraTerm, however nothing seems to be displaying on the screen.
After some thought, I realised what I have done was to load was a SBSFU binary for the H753ZI onto my H745ZI but with just a change to the tamper pin configuration.
At the moment I am trying to figure out how to configure the sample project to compile with the necessary files to run on the H753ZI.
Is there some linker that I need to change to tell the SBSFU to use H745ZI drivers or some configuration somewhere?
Or could the issue also be linked to the fact that the H754ZI is a dual core chip whilst the H753ZI is a single core?
Does anyone have some sample projects that I could reference to point me in the right direction on how to port the examples to another board sucessfully.
It doesnt necessarily have to be the H745ZI but could be from another example like the NUCLEO-L476RG to another board.
Thanks in advance for any help.