Regarding Encryption and Decryption Processing with STSAFE-A110
I am conducting operational verification of the sample application of X-CUBE-SAFEA1 by connecting NUCLEO-L476RG and X-NUCLEO-SAFEA1B.
I have some questions regarding the operation of the sample application "STSAFEA1_WRAP_UNWRAP".
My questions are as follows:
- I demonstrated the sample applcation of "STSAFEA1_WRAP_UNWRAP" with a logic analyzer observing the I2C communication. According to that, it seems that the encryption and decryption processes are performed on the NUCLEO-L476RG side. Is this correct behavior?
- Is it possible to perform encryption and decryption processes on the STSAFE-A110 side (and with secret keys stored in STSAFE-A110)? If so, how can this be implemented?
Details
Below are the steps I have taken:
1. Execution of the sample code
I created a project on STM32CubeIDE via STM32CubeMX and executed the sample application "STSAFEA1_WRAP_UNWRAP" from X-CUBE-SAFEA1. The UART output results appear to be functioning without errors.

2. Step execution with a debugger and observation of I2C communication with a logic analyzer
I performed step execution of the sample application "STSAFEA1_WRAP_UNWRAP" with a debugger and observed the encryption and decryption processes.
It appears that the encryption process is executed in the StSafeA_DataEncryption function at line 2618 of "stsafea_core.c". Similarly, the decryption process seems to be executed in the StSafeA_DataDecryption function at line 2747 of "stsafea_core.c".
StSafeA_ResponseCode_t StSafeA_WrapLocalEnvelope(
StSafeA_Handle_t *pStSafeA,
uint8_t InKeySlotNum,
uint8_t *pInData,
uint16_t InDataSize,
StSafeA_LVBuffer_t *pOutLVResponse,
uint8_t InMAC,
uint8_t InHostEncryption)
{
// ...
/* Encrypt data */
if (((uint8_t)InHostEncryption & (uint8_t)STSAFEA_ENCRYPTION_COMMAND) == (uint8_t)STSAFEA_ENCRYPTION_COMMAND)
{
status_code = StSafeA_DataEncryption(pStSafeA);
}
// ...
}
StSafeA_ResponseCode_t StSafeA_UnwrapLocalEnvelope(
StSafeA_Handle_t *pStSafeA,
uint8_t InKeySlotNum,
uint8_t *pInLocalEnvelope,
uint16_t InLocalEnvelopeSize,
StSafeA_LVBuffer_t *pOutLVResponse,
uint8_t InMAC,
uint8_t InHostEncryption)
{
// ...
/* Decrypt data */
if (((uint8_t)InHostEncryption & (uint8_t)STSAFEA_ENCRYPTION_RESPONSE) == (uint8_t)STSAFEA_ENCRYPTION_RESPONSE)
{
status_code = StSafeA_DataDecryption(pStSafeA);
}
// ...
}
During the execution of each function, I could not observe I2C communication between NUCLEO-L476RG and STSAFE-A110, and it seems that the encryption and decryption processes are performed on the NUCLEO-L476RG side.
3. Confirmation from the datasheet
I referred to the STSAFE-A110 datasheet.
According to Figure 12 "Wrap/Unwrap Local Envelop command flow" on page 21 of the datasheet, it seems that the encryption and decryption of plaintext are processed on the local host(here, NUCLEO-L476RG) side.
On the other hand, the command set list on page 23 includes Encrypt and Decrypt, indicating that STSAFE-A110 seems to provide encryption and decryption functions. Are there commands not implemented in the software of X-CUBE-SAFEA1?
Thank you for your confirmation and response.