Hi @ANaga.2
Please try this command" -c port=swd -ob displ "then tell me the output to check the issue.
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer-2.5.0\bin>STM32_Programmer_CLI.exe -c port=swd -ob displ
-------------------------------------------------------------------
STM32CubeProgrammer v2.5.0
-------------------------------------------------------------------
ST-LINK SN : 0669FF303435554157042733
ST-LINK FW : V2J30M19
Board : NUCLEO-L476RG
Voltage : 3.26V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x415
Revision ID : Rev 4
Device name : STM32L4x1/STM32L475xx/STM32L476xx/STM32L486xx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M4
UPLOADING OPTION BYTES DATA ...
Bank : 0x00
Address : 0x40022020
Size : 20 Bytes
██████████████████████████████████████████████████ 100%
Bank : 0x01
Address : 0x40022044
Size : 16 Bytes
██████████████████████████████████████████████████ 100%
OPTION BYTES BANK: 0
Read Out Protection:
RDP : 0xAA (Level 0, no protection)
BOR Level:
BOR_LEV : 0x0 (BOR Level 0, reset level threshold is around 1.7 V)
User Configuration:
nRST_STOP : 0x1 (No reset generated when entering Stop mode)
nRST_STDBY : 0x1 (No reset generated when entering Standby mode)
nRST_SHDW : 0x1 (No reset generated when entering the Shutdown mode)
IWDG_SW : 0x1 (Software independant watchdog)
IWDG_STOP : 0x1 (IWDG counter active in stop mode)
IWDG_STDBY : 0x1 (IWDG counter active in standby mode)
WWDG_SW : 0x1 (Software window watchdog)
BFB2 : 0x0 (Dual-bank boot disable)
nBOOT1 : 0x1 (Boot from Flash if BOOT0 = 0, otherwise system memory)
SRAM2_PE : 0x1 (SRAM2 parity check disable)
SRAM2_RST : 0x1 (SRAM2 is not erased when a system reset occurs)
PCROP Protection (Bank 1):
PCROP1_STRT : 0xFFFF (0x807FFF8)
PCROP1_END : 0x0 (0x8000000)
PCROP_RDP : 0x0 (PCROP zone is kept when RDP is decreased)
Write Protection (Bank 1):
WRP1A_STRT : 0xFF (0x807F800)
WRP1A_END : 0x0 (0x8000000)
WRP1B_STRT : 0xFF (0x807F800)
WRP1B_END : 0x0 (0x8000000)
OPTION BYTES BANK: 1
PCROP Protection (Bank 2):
PCROP2_STRT : 0xFFFF (0x80FFFF8)
PCROP2_END : 0x0 (0x8080000)
Write Protection (Bank 2):
WRP2A_STRT : 0xFF (0x80FF800)
WRP2A_END : 0x0 (0x8080000)
WRP2B_STRT : 0xFF (0x80FF800)
WRP2B_END : 0x0 (0x8080000)
Best regards,
Nesrine