SBSFU not detecting Active Slot Image
I'm working on integrating the latest SBSFU (v2.6.2) onto an STM32L4A6 platform. I've reviewed both the user manual and application note for the SBSFU, as well as the examples provided.
In my use case:
- I have an external attached MMC flash
- I'm not planning to use the internal MCU flash dual-bank capability (so I can have an image larger than half the 1MB flash size)
- I don't need rollback/swap capability
- For OTA updates, my user application will download the encrypted image to a location in the external MMC flash. The SBSFU on boot will check for a valid image in that location, and if so, it will copy it to the MCU flash active slot.
I was able to get the B-L475E-IOT01A 2_Images_ExtFlash example to boot and run on my board, and it executes the UserApp.
For porting the SBSFU to integrate with my custom UserApp I have:
- Started from the B-L475E-IOT01A 2_Images_ExtFlash example because it seemed like the closest for what I needed.
- Replaced the example QSPI driver with an MMC flash driver
- Modified the various linker files how I think they should be modified based on the user manual/app note.
- Temporarily disabled all security protections in the SBSFU and enabled verbose debugging
- The example I started from with external flash was putting the FIREWALL NVDATA section in the middle of the MCU flash (0x8080000) as if we were using dual-bank internal flash, so I changed that by referencing the NUCLEO-L432KC 1_Image example which uses the Firewall but places the NVDATA section at the start of the first active slot (0x8020000).
- I'm able to build the SECoreBin, SBSFU, and custom UserApp successfuly.
- When I try to use STMCubeProgrammer to flash the resulting combined binary in to the MCU, it loads but it fails to detect a valid image in Active Slot 1 (the master slot), and then it erases that slot because no valid image was found.
- I'm having trouble figuring out why it's not seeing a valid image in that location, since it should be part of the combined binary produced by the SBSFU scripts.
- I've added some trace statements to the when SFU_IMG_DetectFW() is called and more specifically for the SFU_LL_FLASH_INT_Read() function.
- I can see that when it's searching inside the header region, the se_status returns SE_KO, and the se_ret_status returns SE_ERROR, but I'm not sure how to troubleshoot this further.
- Here's a console output from some trace logging I've added in this region:
SFU_IMG_DetectFW -> slot 1
SFU_LL_FLASH_Read internal
Looking in header
pSource: 0x0x8020000, Length: 320 -> pdest: 0x0x20017e78
DoubleECC_Error_Counter: 0
se_status: 1245757
se_ret_status: 100249
SFU_IMG_DetectFW -> slot 1
SFU_LL_FLASH_Read internal
Looking in header
pSource: 0x0x8020000, Length: 320 -> pdest: 0x0x20017e78
DoubleECC_Error_Counter: 0
se_status: 1245757
se_ret_status: 100249
Slot SLOT_ACTIVE_1 not empty : erasing ...
Trying to figure out what my next steps should be to determine why the SBSFU is not finding a valid image in active slot 1.
Thanks!