Setting product state CLOSED without keys loaded
Hello,
I have done a big mistake. I was testing a provisioning using the system bootloader. For that I have changed the provisioning batch files. As a result I have set the product state to closed, before the keys where loaded.
Now I can not connect to the target and the standard regression does not work. Is there a way to get the device working again?
Best regards,
Roman
Here the log:
10:48:50 : Start Debug Authentication Sequence
10:48:50 : SDMOpen : 602 : open : SDM API v1.0
10:48:50 : SDMOpen : 603 : open : SDM Library version v1.1.0
10:48:50 : open_comms : 495 : open : Asserting target reset
10:48:50 : open_comms : 499 : open : Writing magic number
10:48:50 : open_comms : 509 : open : De-asserting target reset
10:48:50 : open_comms : 561 : open : Communication with the target established successfully
10:48:50 : discovery: target ID.......................:0x484
10:48:50 : discovery: SoC ID..........................:0x00000000_38363236_33325117_003D005E
10:48:50 : discovery: SDA version.....................:2.4.0
10:48:50 : discovery: Vendor ID.......................:STMicroelectronics
10:48:50 : discovery: PSA lifecycle...................:ST_LIFECYCLE_CLOSED
10:48:50 : discovery: PSA auth version................:1.0
10:48:50 : discovery: ST HDPL1 status.................:0x1
10:48:50 : discovery: ST HDPL2 status.................:0xffffffff
10:48:50 : discovery: ST HDPL3 status.................:0xffffffff
10:48:50 : discovery: Token Formats...................:0x200
10:48:50 : discovery: Certificate Formats.............:0x201
10:48:50 : discovery: cryptosystems...................:Ecdsa-P256 SHA256
10:48:50 : discovery: ST provisioning integrity status:0xf5f5f5f5
10:48:50 : discovery: permission if authorized...........:Full Regression
10:48:50 : discovery: permission if authorized...........:To TZ Regression
10:48:50 : discovery: permission if authorized...........:Level 3 Intrusive Debug
10:48:50 : discovery: permission if authorized...........:Level 2 Intrusive Debug
10:48:50 : discovery: permission if authorized...........:Level 1 Intrusive Debug
10:48:50 : discovery: permission if authorized...........:Level 3 Intrusive Non Secure Debug
10:48:50 : discovery: permission if authorized...........:Level 2 Intrusive Non Secure Debug
10:48:50 : discovery: permission if authorized...........:Level 1 Intrusive Non Secure Debug
10:53:32 : UR connection mode is defined with the HWrst reset mode
10:53:32 : ST-LINK SN : 004A00233232511639353236
10:53:32 : ST-LINK FW : V3J12M3
10:53:32 : Board : STM32H573I-DK
10:53:32 : Voltage : 3.26V
10:53:32 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication