SHCI_C2_FUS_LoadUsrKey doesn't load AES1 key registers
Hi all
I'm working on a STM32WB55 nucleo board
I'm designing a simple Signing procedure
At beginning I've try that every thing ok by using a hard codded key and now I want to switch on a key kept secure in FUS zone
I've load 2 256 bits AES keys into FUS user Key secure zone first time with a custom app that will be loaded in prod to set all default keys
second time I've try by cube programmer
I've based my procedure on CKS example
- call HAL_CRYP_DeInit() to clear all AES regs and context
- setup handle.init structure : I'm initializing for a 32 bytes buffer input and AES CBC mode
- call HAL_CRYP_Init() and keeping AES key to NULL (to avoid HAL_CRYP_Encrypt() call overwrite AES KEY registers
- call SHCI_C2_FUS_LoadUsrKey() with the good key index
- call HAL_CRYP_Encrypt()
- finaly unload the key etc ...
if I use 1 or 2 as index SHCI_C2_FUS_LoadUsrKey() is responding SHCI_Success
if I use another index not previously set with a key it's answering SHCI_FUS_CMD_NOT_SUPPORTED
it makes me feel that keys have been correctly wrote to FUS secure zone and when I ask wireless stack to bring me back the keys it's understanding what I'm willing
unfortunately after SHCI_C2_FUS_LoadUsrKey() call noting is wrote into AES KEYR*
I've surely missed something but can't figure what
here you can find my piece of code
// get the SHA_256 hash of FW binary image
SIG_HASH_INIT(&hasher);
SIG_HASH_UPDATE(&hasher,BOOTLOADER_START_APP_ADDRESS,Bootloader_shared_infos_RAM.fwByteSize);
SIG_HASH_DIGEST(&hasher,Bootloader_shared_infos_RAM.Computed_key);
// uint32_t key[]={0x00000000,0x00000000,0x00000000,0x00000000,
// 0x00000000,0x00000000,0x00000000,0x00000000};
uint32_t iv[] ={Bootloader_shared_infos_RAM.Descriptor,Bootloader_shared_infos_RAM.Descriptor,Bootloader_shared_infos_RAM.Descriptor,Bootloader_shared_infos_RAM.Descriptor};
hcryp1.Instance = AES1;
if (HAL_CRYP_DeInit(&hcryp1) != HAL_OK)
return RETURN_ERROR;
hcryp1.Init.DataType = CRYP_DATATYPE_8B;
hcryp1.Init.DataWidthUnit = CRYP_DATAWIDTHUNIT_BYTE;
hcryp1.Init.KeySize = CRYP_KEYSIZE_256B;
hcryp1.Init.Algorithm = CRYP_AES_CBC;
//hcryp1.Init.pKey = key; /* Key will be provided by CKS service */
hcryp1.Init.pKey=NULL; // should be published at next step by FUS himself
hcryp1.Init.HeaderWidthUnit = CRYP_HEADERWIDTHUNIT_WORD;
hcryp1.Init.KeyIVConfigSkip = CRYP_KEYIVCONFIG_ALWAYS;
hcryp1.Init.pInitVect = iv;
if (HAL_CRYP_Init(&hcryp1) != HAL_OK)
return RETURN_ERROR;
printf("load Bootloader Key :");
SHCI_CmdStatus_t res=SHCI_C2_FUS_LoadUsrKey(1); // should write key #1 into AES_KEY_R*
print_SHCI_CmdStatus_t(res);// with index 1/2 i get SHCI_Success return with anything else I get Unknown Cmd answer (looks ok as only first and 2nd key are wrotes
/// when looking in AES_KEYR* reg at this step they are still at 0
uint8_t cyphered[BOOTLOADER_APP_SIGNATURE_SIZE];
if (HAL_CRYP_Encrypt(&hcryp1, Bootloader_shared_infos_RAM.Computed_key, BOOTLOADER_APP_SIGNATURE_SIZE,cyphered, 0xFF) != HAL_OK)
return RETURN_ERROR;
thanks for any idea that would come to your mind