Signature generated by stm crypto lib different from a signature generated by python for the same key
I am trying to create a mechanism of verification where I sign a file on the PC save it to a disk on a key device and then verify it by the MCU after saving it to internal flash.
The PC is doing the signing process and the MCU should only do the verification process.
On the PC side I sign the image with the pkcs1_15.sign() function from the pycryptodome library.
On the MCU is the public key is saved as modulus and exponent in the following format:
unsigned char RSAKeyModulus[] = {
// Offset 0x00000000 to 0x00000158
0x30, 0x81, 0x9F, 0x30, 0x0D, 0x06, 0x09, 0x2A, 0x86, 0x48, 0x86, 0xF7,
0x0D, 0x01, 0x01, 0x01, 0x05, 0x00, 0x03, 0x81, 0x8D, 0x00, 0x30, 0x81,
0x89, 0x02, 0x81, 0x81, 0x00, 0xD6, 0x35, 0x43, 0x7C, 0xC9, 0x22, 0x18,
0x16, 0xF5, 0xE9, 0xB9, 0x29, 0x51, 0x80, 0x3F, 0x1D, 0xC0, 0x94, 0xCF,
0x91, 0x0D, 0x38, 0x6E, 0x83, 0x51, 0x22, 0x52, 0xC0, 0x8D, 0xBD, 0xD3,
0x21, 0x68, 0x52, 0x50, 0x39, 0x79, 0xC6, 0x6D, 0x19, 0x9B, 0xFE, 0x61,
0xDF, 0xFA, 0xB3, 0x7E, 0xE1, 0x71, 0xA9, 0xE2, 0x3C, 0x72, 0xDA, 0x78,
0x79, 0xCF, 0xAC, 0x3C, 0x76, 0xC1, 0xFF, 0xCC, 0x3D, 0xBF, 0xBD, 0xE4,
0x71, 0x34, 0xA4, 0x9D, 0xD3, 0x3B, 0xD8, 0x3B, 0x11, 0x18, 0x6B, 0x82,
0x6F, 0x65, 0xAB, 0xCC, 0x2A, 0x6A, 0xC6, 0x10, 0x43, 0x15, 0xE5, 0xC4,
0x52, 0x67, 0x56, 0x45, 0xD6, 0x31, 0x7D, 0x29, 0x33, 0x27, 0x5D, 0xB6,
0xF5, 0xBB, 0x83, 0xAC, 0x49, 0xCB, 0xD2, 0xF8, 0xF3, 0x39, 0x0B, 0x92,
0x3A, 0xBD, 0x5C, 0x0B, 0xB8, 0x13, 0x87, 0xFD, 0xA2, 0xCF, 0x3F, 0x5E,
0xB5, 0x02, 0x03
};
unsigned char RSAPublicExponent[] = {
0x01, 0x00, 0x01
};That was generated from the same private key used to sign the image.
I'm downloading the file to the MCU and calculating the hash(sha-256) value and receive the same hash value as calculated on the PC side by python.
But the verification function(RSA_PKCS1v15_Verify) called with the has value and the expected signature returns SIGNATURE_INVALID.
To try and solve the problem I added the private key to the code and calculated the signature on the MCU. The sign function(RSA_PKCS1v15_Sign) generated a different key from the one generated with python on the PC. and calling the verify function for this signature returned SIGNATURE_VALID.
I'm guessing there is some difference in the RSA parameters between the python function and ST function.
I will be glad for any suggestions about what can solve the problem.