Skip to main content
Associate III
June 2, 2025
Question

Start Securing Features with STM32H533

  • June 2, 2025
  • 2 replies
  • 2624 views

Hi,

 

I would like to work with the security features of STM32H533RE microcontroller. For that,

1.Do I need to enable anything or install any libraries files in order to work with it.

2. If there is any example projects available?

3. The path for Installation and documents .

Please help me out.

2 replies

TDK
Super User
June 2, 2025

There are a bunch of examples here. Several of them deal with security features. These can likely be loading with the Example Selector in CubeMX/CubeIDE

STM32CubeH5/Projects/NUCLEO-H533RE at main · STMicroelectronics/STM32CubeH5

"If you feel a post has answered your question, please click ""Accept as Solution""."
Jocelyn RICARD
ST Employee
June 4, 2025

Hello @Keerthi ,

I would alsa advise having a look to the wiki here

Best regards

Jocelyn

 

KeerthiAuthor
Associate III
June 5, 2025

Hi, 

I will go through it. STM32H533RE Nucleo board i am using it does not support secure Manager. If that is the case, How would I store the keys such that i cant be accessible. Is it possible to generate the keys.