Skip to main content
Associate
April 1, 2026
Question

STiROT + OEMuROT for STM32H7S startup on XIP project

  • April 1, 2026
  • 0 replies
  • 95 views

Hello,

After spending several days investigating this topic and reviewing all the documentation I could find, I am still completely stuck on how to proceed with implementing STiROT + OEMuROT on my STM32H7S3.

An important point is that I am trying to add this security architecture to a project that is already at a fairly advanced stage of development. The project was originally built on top of the XIP template provided by ST:

https://github.com/STMicroelectronics/STM32CubeH7RS/tree/main/Projects/NUCLEO-H7S3L8/Templates/Template_XIP 

The difficulty comes from the fact that, in the XIP context, the project only includes these layers:

  • Appli
  • Boot
  • ExtMemLoader

As a first step, I imported ROT_Provisioning into the project in a separate folder. However, I still do not see how I should properly integrate or adapt the following components into my current project structure:

  • OEMiROT_Appli
  • OEMiROT_Boot
  • STiROT_Appli
  • STiROT_Boot

Should I try to merge the `*_Appli` projects into my existing Appli context, and the `*_Boot` projects into my existing Boot context? Or is the expected approach different when starting from the XIP template?

I also reviewed the following ST Wiki article, which seems relevant to this type of use case, but I still could not find a clear way forward:

https://wiki.st.com/stm32mcu/wiki/Security:How_to_adapt_a_user_application_to_ROT_for_STM32H7RS#STM32CubeIDE-0 

At this point, what I am mainly missing is a clear starting methodology for adapting an advanced XIP-based project to a setup that includes STiROT + OEMuROT.

Any guidance, recommended project structure, migration steps, or example workflow would be greatly appreciated.

Thank you very much in advance for your time and help and best regards!