STM32 Cyptolib with IAR 8.11
Posted on April 13, 2017 at 09:11
I've my application that uses the xCube CyptoLib 3.1.0 (STM32CryptographicV3.0.0_CM4_IAR_otnsc.a)with IAR compiler. Up to version 8.10 of the IAR compiler I never had any warning or error during the build of the project. Upgrading the IAR IDE to version 8.11 I have this error:
'Warning[Lt009]: Inconsistent wchar_t size crypto.o(STM32CryptographicV3.0.0_CM4_IAR_otnsc.a) has wchar_t size 16 bits '
Reading the release notes of the IAR 8.11 I found this:
IAR Information Center for ARM
Changed size of wchar_t in version 8.10 and 8.11
Object files following the ARM ABI has a runtime attribute indicating the size of wchar_t.
In EWARM version 7.80 and earlier, the size of wchar_t was 2 bytes wide and the runtime attribute was set accordingly.
For EWARM version 8.10, the size of wchar_t was 4 bytes wide but the value of the runtime attribute was not updated. Thus in 8.10 code is generated with 4 byte wide wchar_t but the object file is marked as if wchar_t is 2 bytes wide.
In EWARM version 8.11 wchar_t is 4 bytes wide and the runtime attribute is set accordingly.
Looking only at the wchar_t aspect this has the following implications:
All good except need to remove all parent title text for all comments.
Need to remove all parent title text for all comments.
- Combining object files built with 7.80 and 8.10 will not trigger any linker warning but if the application uses wchar_t, the behavior will be unpredictable.
- Combining object files built with 8.10 and 8.11 will trigger a linker warning but the application should work even if it uses wchar_t.
- Combining object files built with 7.80 and 8.11 will trigger a linker warning and if the application uses wchar_t, the behavior will be unpredictable.
Then, by this description, theCryptoLib 3.1.0 needs to be rebuilded with new version of the compiler to avoid unpredictable issues.
I planned a new release of the Crytolib compiled with IAR 8.11?
How I can solve this issue?
Thanks