Stm32 linux crypto question not start @ main
Hi , i am new to linux,
i am using crypto 3.0 package and stm32F205xx and
encounter several problem :
i write my own makefile and linker script (mostly copy from guthub)
I use stlink-texane and gdb to debug, here are several question:
1)
Type ''apropos word'' to search for commands related to ''word''...
Reading symbols from main.elf...done.(gdb) tar ext:4242Remote debugging using :42420x08000354 in SystemInit () at system_stm32f2xx.c:154154 RCC->CR &= (uint32_t)0xFFFBFFFF;(gdb) s157 RCC->CIR = 0x00000000;(gdb) ss169 }I was wonder why it don't start @ main.c
Anything i would come wrong?
2) I try to apply some simple test say i add some variable
unsigned char test = 100 @ line 100
and then once i debug
''b main.c:100'' and continue
when i use ''p test'' (which i expected it come out 100, it gives another value
I would please if anyone can help.
Thanks
2)