STM32H5 simple security settings
Hi,
I have a question about choosing some fairly basic security settings for an STM32H5.
We are developing a system that uses both G4 and H5 micros. We have developed a largely common bootloader that receives a signed encrypted application over variously USB, UART, or CAN, and flashes it to internal memory. This is working on the G4 and H5.
For the G4, we understand that if we select "Level 1" read protection, the bootloader will still be able to erase and re-flash a new application but a user will not be able to gain access to the code (bootloader, application, or data in CC RAM). Further, the G4 can be reverted to Level 0 if required, but this will erase the proprietary code.
Ideally, we would like the same security behaviour on the H5. I have been reading about the bewildering selection of security settings with privileged and secure settings for individual peripherals but I feel this is more complicated than we require. Our bootloader already prevents someone installing malicious code so I believe we just need a means of locking out the JTAG port to prevent someone reading the bootloader or decrypted application from flash. Ideally we would like this security setting to be reversible but with a full chip erase, as on the G4.
I would be grateful for any advice on suitable security setting.
Thanks