STM32H563 I2C doesn't work when TrustZone enabled with OEMiROT boot path.
Hello,
I am working on implementing secure firmware with OEMiRoT boot on the STM32H563. I have configured I2C1 and TIM1 as non-secure peripherals. While the TIM1 interrupt works as expected, I am encountering an issue where the I2C1 slave interrupt handler is never entered. (Note: The I2C slave works correctly if TrustZone is disabled.)
I am wondering if the I2C1 slave interrupt handler requires special handling when configured as a non-secure peripheral with TrustZone enabled?
Additionally, if I need to change the start offset and application size for secure and non-secure applications, what changes are required beyond updating flash_layout.h in OEMiROT project?
Any assistance on these issues would be greatly appreciated.
Thanks,
Ivan