Skip to main content
BRIAN_LAI
Associate II
May 15, 2024
Question

Stm32H563MI OBKey Provisioning failed problem and PRODUCT_STATE

  • May 15, 2024
  • 1 reply
  • 1047 views

Hi, I just accidentally modified the PRODUCT_STATE to provisioning and not able to recover.

BRIAN_LAI_1-1715768360017.png

So, I tried to do the OBKey Provisioning and use DA to regression back to Open State.

I've created my OBKey:

BRIAN_LAI_2-1715768568514.png

However, provisioning always failed.

BRIAN_LAI_3-1715768680743.png

Is there any other settings need to be turned off for OBKey Provisioning?
Or is there any other way to turn PRODUCT_STATE back to OPEN again?

 

1 reply

Jocelyn RICARD
ST Employee
May 30, 2024

Hello @BRIAN_LAI ,

with STM32H56x you shouldn't use encryption.

This may be the reason why it fails.

In fact this is strange that encryption is enabled. If you use the files from STM32Cube_FW_H5_V1.2.0\Projects\NUCLEO-H563ZI\ROT_Provisioning\DA\Config\DA_ConfigWithPassword.xml you will see that it is disabled.

Another way to go is to use the default password provided in STM32CubeProgrammer here: C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\DA_Default_Config\STM32H5\NonCrypto\DA_Config_Password.obk

You can try provision this OBK and then use C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\DA_Default_Config\STM32H5\password.bin to re-open

Best regards

Jocelyn