STM32H573 stuck in PROVISIONING state
Hi there,
My STM32H573I-DK demo board is stuck in PROVISIONING state, probably as the result of a failed or aborted provisioning operation. I was doing hand-on training with the How to start with STiRoT on STM32H573 wiki.
Now, I cannot regress it to OPEN, or run the provisioning.sh script again to proceed to CLOSED. Any attempt ends up in a Debug Authentication Failed error.
I am aware of the importance of providing DA credentials to avoid locking the device in CLOSED state. But I don't think I missed this step, and my device is not CLOSED.
Any idea how I can unlock this board ?
Thanks for any support.
Christian R
FYI, here is the log of a regression attempt using STM32Programmer:
09:34:22 : STM32CubeProgrammer API v2.17.0 | Linux-64Bits
09:34:40 : Start Debug Authentication Sequence
09:34:40 : SDMOpen : 609 : open : SDM API v1.0
09:34:40 : SDMOpen : 610 : open : SDM Library version v1.1.0
09:34:40 : open_comms : 501 : open : Asserting target reset
09:34:40 : open_comms : 505 : open : Writing magic number
09:34:40 : open_comms : 515 : open : De-asserting target reset
09:34:40 : open_comms : 567 : open : Communication with the target established successfully
09:34:40 : discovery: target ID.......................:0x484
09:34:40 : discovery: SoC ID..........................:0x00000000_35353537_3332510A_00680036
09:34:40 : discovery: SDA version.....................:2.4.0
09:34:40 : discovery: Vendor ID.......................:STMicroelectronics
09:34:40 : discovery: PSA lifecycle...................:ST_LIFECYCLE_PROVISIONING
09:34:40 : discovery: PSA auth version................:1.0
09:34:40 : discovery: ST HDPL1 status.................:0xffffffff
09:34:40 : discovery: ST HDPL2 status.................:0xffffffff
09:34:40 : discovery: ST HDPL3 status.................:0xffffffff
09:34:40 : discovery: Token Formats...................:0x200
09:34:40 : discovery: Certificate Formats.............:0x201
09:34:40 : discovery: cryptosystems...................:Ecdsa-P256 SHA256
09:34:40 : discovery: ST provisioning integrity status:0xf5f5f5f5
09:34:40 : discovery: permission if authorized...........:Full Regression
09:34:40 : discovery: permission if authorized...........:To TZ Regression
09:34:40 : discovery: permission if authorized...........:Level 3 Intrusive Debug
09:34:40 : discovery: permission if authorized...........:Level 2 Intrusive Debug
09:34:40 : discovery: permission if authorized...........:Level 1 Intrusive Debug
09:34:40 : discovery: permission if authorized...........:Level 3 Intrusive Non Secure Debug
09:34:40 : discovery: permission if authorized...........:Level 2 Intrusive Non Secure Debug
09:34:40 : discovery: permission if authorized...........:Level 1 Intrusive Non Secure Debug
09:35:11 : Start Debug Authentication Sequence
09:35:11 : SDMOpen : 609 : open : SDM API v1.0
09:35:11 : SDMOpen : 610 : open : SDM Library version v1.1.0
09:35:11 : open_comms : 501 : open : Asserting target reset
09:35:11 : open_comms : 505 : open : Writing magic number
09:35:11 : open_comms : 515 : open : De-asserting target reset
09:35:11 : open_comms : 567 : open : Communication with the target established successfully
09:35:11 : [00%] discovery command
09:35:11 : [10%] sending discovery command
09:35:11 : [20%] receiving discovery
09:35:11 : [40%] loading credentials
09:35:11 : [50%] sending challenge request
09:35:11 : [60%] receiving challenge
09:35:11 : Error: Debug Authentication Failed