Skip to main content
bpentz
Associate
March 14, 2019
Question

STM32H7 Flash Bank CRC

  • March 14, 2019
  • 1 reply
  • 838 views

I am trying to use the hardware CRC built into the embedded flash module. When I use the start and end addresses and kick off the CRC, the processor halts and I have to do a full flash erase to get it back. Are the start and end addresses relative to the base of the flash bank? Here is my code:

 
// Unlock FLASH_CR1/2 register
FLASH->KEYR1 = 0x45670123;
FLASH->KEYR1 = 0xcdef89AB;
 
// Enable the CRC feature by setting CRC_EN in FLASH_CR1/2
FLASH->CR1 |= FLASH_CR_CRC_EN;
 
// Lock the CR1/2 register
FLASH->CR1 |= FLASH_CR_LOCK;
 
// Set crc burst length to 01: 64 flash words (64 * 32 bytes/word = 2048 bytes)
// In the link script, the binary must end on a 2048 byte boundary in this case
FLASH->CRCCR1 &= ~FLASH_CRCCR_CRC_BURST_Msk;
FLASH->CRCCR1 |= FLASH_CRCCR_CRC_BURST_0;
 
// Check CRC between defined addresses, not by sector
FLASH->CRCCR1 &= ~FLASH_CRCCR_CRC_BY_SECT;
//	FLASH->CRCCR1 |= FLASH_CRCCR_CRC_BY_SECT;
 
// Set start and end addresses, relative to the start of this flash bank
// (i.e. address 0x8000000 is 0 on bank 1)
FLASH->CRCSADD1 &= ~FLASH_CRCSADD_CRC_START_ADDR_Msk;
FLASH->CRCSADD1 = 0;
FLASH->CRCEADD1 &= ~FLASH_CRCEADD_CRC_END_ADDR_Msk;
//	FLASH->CRCEADD1 = (((uint32_t)&_ebin) - ((uint32_t)&_bflash)) & FLASH_CRCEADD_CRC_END_ADDR_Msk;
FLASH->CRCEADD1 = 0x80;
 
// Start CRC
FLASH->CRCCR1 |= FLASH_CRCCR_START_CRC;
 
 
// Wait on CRC_BUSY in FLASH_SR
while(FLASH->SR1 & FLASH_SR_CRC_BUSY);
x = FLASH->SR1 & FLASH_SR_CRC_BUSY;

It halts on line 30. I've tried a number of start and end addresses.

This topic has been closed for replies.

1 reply

flyer31
Senior
May 20, 2019

I have the same problem with trying "FLASH_CRCCR_ALL_BANK" (STM32H750 Rev Y).

My SYSTICK interrupt continues working. If WWDG or IWDG are enabled, they will lead to reset... . But otherwise the controllers hangs completely - it needs new reset. (I have DCACHE and ICACHE enabled ... maybe this is the problem? ... but I did not try further, I can also calculate the CRC manually, no problem).