STM32L151CC with OPTVERR = 1
I'm trying to enable the OB_RDP_Level_1 for a STM32L151CC but It fails. The MCU becomes bricked. I can't even boot to DFU. I need to first start ST link utility and set read out protection level 0, and then do a chip erase.
But I noticed that bit OPTVERR = 1 indicating that the option bytes are faulty. I have tried a fulle chip erase and it does not set the OPTVERR to zero. Is it possible that I have a special STM32 that always start up with OPTVERR = 1?
I have tested on some evaluation boards and they have OPTVERR = 0 at start.