STM32L4 readout protection RDP
Using STM32L452CC and STM32CubeProgrammer API v2.12.0 Windows 64-bits.
Firstly, I'm setting the readout protection to its middle level (RDP = BB in the programmer) and then program the chip successfully. Then, letting the chip power cycle. Now reading the option bytes from CubeProgrammer but getting AA, Any idea?
Another related question:
My understanding is that if the protection level is set to BB (protection level 1) then Cube programmer will still be able to program a new firmware to the chip and have the protection level being downgraded to AA (no protection).
However, this is denied by CubeProgrammer Command-interface.
It just let the new firmware to be programmed, but not downgrading the protection level to be 'no protection. Any idea?