STM32U5 RDP2 password accepted but ST-Link fails: DEV_TARGET_NOT_HALTED
Hello ST Community,
I am working with an STM32U5 based board and facing serious issue related to RDP Level 2 and debug access. I am attempting to recover the device using STM32 Programmer CLI and Cube Programmer but it is not responding as expected even after a successful RDP2 password unlock.
$ STM32_Programmer_CLI.exe -c port=swd mode=UR -unlockrdp2 0x18BBDDEF 0x19CCBBEF
-------------------------------------------------------------------
STM32CubeProgrammer v2.19.0
-------------------------------------------------------------------
ST-LINK SN : 003200253133510636303739
ST-LINK FW : V3J15M7B5S1
Board : STLINK-V3SET
Voltage : 3.54V
Error: Unable to get core ID
Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
Error: Unable to get core ID
ST-LINK SN : 003200253133510636303739
ST-LINK FW : V3J15M7B5S1
Board : STLINK-V3SET
Voltage : 3.54V
Unlock RDP2 password successfully done
Error: ST-LINK error (DEV_TARGET_NOT_HALTED)
I need help with:
1. why is the core still inaccessible even after RDP2 unlock?
2. Is the device stuck due to TrustZone configuration or another misconfiguration?
3. Solution on above configuration