STM32U5 SAES/AES shared key in Trustzone with HAL
Hello,
I'm trying to use the SAES/AES shared key functionality in a Trustzone (TZEN=1, RDP = 0), using the functions provided by the HAL library. The board I use is the B-U585I-IOT02A.
The only project example I found is with Trustzone disabled, but it runs correctly with my configuration (TZEN=1, RDP = 0) without any changes. Just one executable image loaded running in non-secure (without the secure - non secure switch).
The code is roughly the following (I removed checks and key/IV definition):
HAL_Init();
SystemClock_Config();
SystemPower_Config();
MX_ICACHE_Init();
MX_RNG_Init();
hcryp.Instance = SAES;
hcryp.Init.DataType = CRYP_NO_SWAP;
hcryp.Init.KeySize = CRYP_KEYSIZE_256B;
hcryp.Init.pInitVect = (uint32_t *)pInitVectSAES;
hcryp.Init.Algorithm = CRYP_AES_CBC;
hcryp.Init.KeyIVConfigSkip = CRYP_KEYIVCONFIG_ALWAYS;
hcryp.Init.KeyMode = CRYP_KEYMODE_SHARED;
hcryp.Init.KeySelect = CRYP_KEYSEL_HW;
hcryp.Init.KeyProtection = CRYP_KEYPROT_DISABLE;
HAL_CRYP_Init(&hcryp)
HAL_CRYPEx_EncryptSharedKey(&hcryp, AESKey256, Encryptedkey, 0, TIMEOUT_VALUE);
HAL_CRYPEx_DecryptSharedKey(&hcryp, Encryptedkey,0, TIMEOUT_VALUE);
hcryp.Instance = AES;
hcryp.Init.DataType = CRYP_NO_SWAP;
hcryp.Init.KeySize = CRYP_KEYSIZE_256B;
hcryp.Init.KeyMode = CRYP_KEYMODE_SHARED;
hcryp.Init.Algorithm = CRYP_AES_ECB;
HAL_CRYP_Init(&hcryp);
HAL_CRYP_Encrypt(&hcryp, Plaintext, 16, EncryptedText, TIMEOUT_VALUE);
HAL_CRYP_Decrypt(&hcryp, EncryptedText, 16, DecryptedText, TIMEOUT_VALUE);
The problem is when I try to run it in a Trustzone Project starting in secure and switching to non-secure. I tested this code both from secure (before the switch) and non-secure, attributing all the peripherals (AES, SAES, RNG and ICACHE) to the correct security domain (secure or non-secure). When the peripherals were attributed to secure the following lines were added in the GTZC configuration function in the secure main:
HAL_GTZC_TZSC_ConfigPeriphAttributes(GTZC_PERIPH_AES, GTZC_TZSC_PERIPH_SEC|GTZC_TZSC_PERIPH_NPRIV)
HAL_GTZC_TZSC_ConfigPeriphAttributes(GTZC_PERIPH_RNG, GTZC_TZSC_PERIPH_SEC|GTZC_TZSC_PERIPH_NPRIV)
HAL_GTZC_TZSC_ConfigPeriphAttributes(GTZC_PERIPH_SAES, GTZC_TZSC_PERIPH_SEC|GTZC_TZSC_PERIPH_NPRIV)
When I try to use the AES module to perform encryption with the shared key:
HAL_CRYP_Encrypt(&hcryp, Plaintext, 16, EncryptedText, TIMEOUT_VALUE);the operation times out (I checked with the debugger), even if the function returns HAL_OK. The EncryptedText is therefore all zeros.
This is the call order of HAL functions, with WaitOnCCFlag which times out:
HAL_CRYP_Encrypt(&hcryp, Plaintext, 16, EncryptedText, TIMEOUT_VALUE);
static HAL_StatusTypeDef CRYP_AES_Encrypt(CRYP_HandleTypeDef *hcryp, uint32_t Timeout)
static void CRYP_AES_ProcessData(CRYP_HandleTypeDef *hcryp, uint32_t Timeout)
static HAL_StatusTypeDef CRYP_WaitOnCCFlag(CRYP_HandleTypeDef *hcryp, uint32_t Timeout)
I checked that both AES (gcm), SAES (in both Normal and Wrapped key modes, using DHUK) were working, with the same project configuration.
I don't understand why this happens, since the key sharing works for the same board configuration (Opition Bytes) if I just load the non-secure image. Is there some configuration step that I am missing?